Part Number: TCAN1043A-Q1
Is there any relevant data on the delay time of this chip’s internal processing?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1043A-Q1
Is there any relevant data on the delay time of this chip’s internal processing?
Hi Ray,
What signal delay time is of interest here? If it is the CAN signal delay from the TXD input to the CAN pin output or the CAN pins to the RXD output, this is included in the propagation delay timing specifications. Note that the maximum value of these two values combined will be less than the maximum loop delay timing specification.
Is there are different signal that you are wondering about?
Regards,
Eric Schott