Part Number: THVD2452V
Is there a IBIS model for PTHVD2452VDR? If not, is there a equivalent part with a IBIS model I can use?
Thanks,
Thien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Thien,
We don't have an IBIS model for this device.
We do have an ibis model for the THVD2450 which would be the closest device - but it isn't 1:1 equivalent.
Main differences are: It is half duplex instead of full, doesn't have separate logic supplies, and doesn't have a slew rate limit option.
I understand there are important features missing - but this is our closest device electrically and timing wise and should give the most similar results.
Best,
Parker Dodson