Part Number: TDES960
Hi All,
Customers use TDES960.
When using three cameras, the time per line for Bandwidth considering overhead differs between calculation and actual operation.
BW considering overhead was calculated as 5720Mbps from the data sheet.
■Camera specifications
・Active width: 2560pixel
・active height: 1944pixel
・Format: UYVY(16bit/pixel)
・For 3 cameras
→ Bit rate per camera 1906Mbps (5720/3)
→Time per line 21.5us or more (2560*16/1906)
However, if the camera line time is set to 22us, it will not be possible to capture normally.
It works properly when set to 26usec or higher.
The calculation is 21.5usec, but it actually works normally at 26usec. Are there any settings or restrictions?
Best Regards,
Ishiwata