Part Number: DS250DF230
Hi,
1. Only the Typ value is listed, do you have the Max value data? Is it possible to exceed 0.5s or 1s in some cases? Is there a formula for CDR Lock Time?

2. It says Typ <100ms when Normal Lock Mode is 25.78Gbps, but does this value change when it is 9.8304Gbps? If it does, is it longer or shorter?
3. Can you tell me the max value of CDR Lock Time at 9.8304Gbps? Could you tell me the value which is definitely not exceeded, such as max=250ms, 300ms, 400ms?
Best Regards,
Nishie