This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1462-Q1: ISO 11898-2:2023

Part Number: TCAN1462-Q1
Other Parts Discussed in Thread: TCAN1463-Q1, TCAN1043A-Q1

Hi Team,

Does TCAN1462-Q1 meet the requirements of ISO 11898-2:2023 standard? I couldn't find any descriptions in the  datasheet. Please check it and let me know.

Regards,

  • Hi Jeffrey,

    Thanks for reaching out! As of the time of this post, the most recent published ISO standards for CAN and CAN SIC are ISO 11898-2:2016 and CIA 601-4. Currently, the next revision of ISO 11898-2 is in FDIS status, meaning it is not yet published and released.

    Our TCAN1462-Q1 and TCAN1463-Q1 meet the specifications outline in ISO 11898-2:2016 and CIA 601-4. Once the next revision of ISO 11898-2 is released, we will also be sure to keep our portfolio up to date. Currently, our next versions of the TCAN1462-Q1, TCAN1463-Q1, and TCAN1043A-Q1 components are expected to be releasing next year, and they will be follow the most updated standard, which I imagine will be titled either ISO 11898-2:2023 or ISO 11898-2:2024.

    Best,

    Danny

  • Hi Danny,

    Thanks for your kind response. It is very useful information for me.

    Regards,