Part Number: DP83822IF
Other Parts Discussed in Thread: AM6421
We designed a custom board utilizing the AM6421 System on Chip (SOC) for an industrial protocol. where we connected industrial ports (PRU-ICSS) using RGMII to DP83822IFRHBT. Using MDIO we are able to connect and configure PHY in internal Loopback mode (MII). This activity to test connection between SOC to PHY . Please find attached logs for same. Also we are able to probe TX CLK , TX CTRL , TX_DO to TX_D3. We can see signals. Can anyone help from team analyze logs & give us input? Notes - 1) we already confirmed hardware connection strapping option with SOR1 (0x467U) & SOR2 (0x468U) . Its matching. 2) Without Loppback we also tested Link status with Laptop. Its working. We are able to confirm Link status with LED indication & phy register. 3) Energy Efficient Ethernet (EEE) option is enable.
Before LoopBack Enabled
PHY 1: BMCR (0x0000) = 0x3100
PHY 1: BMSR (0x0001) = 0x7849
PHY 1: PHYIDR1 (0x0002) = 0x2000
PHY 1: PHYIDR2 (0x0003) = 0xa240
PHY 1: ANAR (0x0004) = 0x01e1
PHY 1: ANLPAR (0x0005) = 0x0000
PHY 1: ANER (0x0006) = 0x0004
PHY 1: ANNPTR (0x0007) = 0x2001
PHY 1: ANLNPTR (0x0008) = 0x0000
PHY 1: CR1 (0x0009) = 0x0000
PHY 1: CR2 (0x000A) = 0x0100
PHY 1: CR3 (0x000B) = 0x1000
PHY 1: REGCR (0x000D) = 0x0000
PHY 1: ADDAR (0x000E) = 0x0000
PHY 1: FLDS (0x000F) = 0x0000
PHY 1: PHYSTS (0x0010) = 0x4002
PHY 1: PHYSCR (0x0011) = 0x0108
PHY 1: MISR1 (0x0012) = 0x0000
PHY 1: MISR2 (0x0013) = 0x0800
PHY 1: FCSCR (0x0014) = 0x0000
PHY 1: RECR (0x0015) = 0x0000
PHY 1: BISCR (0x0016) = 0x0100
PHY 1: RCSR (0x0017) = 0x0241
PHY 1: LEDCR1 (0x0018) = 0x0400
PHY 1: PHYCR (0x0019) = 0x8021
PHY 1: 10BTSCR (0x001A) = 0x0000
PHY 1: BICSR1 (0x001B) = 0x007d
PHY 1: BICSR2 (0x001C) = 0x05ee
PHY 1: CDCR (0x001E) = 0x0102
PHY 1: PHYRCR (0x001F) = 0x0000
PHY 1: MLEDCR (0x0025) = 0x0000
PHY 1: COMPT (0x0027) = 0x2001
PHY 1: COMPT (0x003E) = 0x0102
PHY 1: PTPCFG (0x003F) = 0x0000
PHY 1: (0x0040) = 0x3100
PHY 1: TXCPSR (0x0042) = 0x2000
EnetPhy_bindDriver: PHY 1: OUI:080028 Model:24 Ver:00 <-> 'dp83822' : OK
PHY 1 is alive
PHY 2 is alive
After LoopBack Enabled
PHY 1: BMCR (0x0000) = 0x6100
PHY 1: BMSR (0x0001) = 0x7849
PHY 1: PHYIDR1 (0x0002) = 0x2000
PHY 1: PHYIDR2 (0x0003) = 0xa240
PHY 1: ANAR (0x0004) = 0x01e1
PHY 1: ANLPAR (0x0005) = 0x0000
PHY 1: ANER (0x0006) = 0x0004
PHY 1: ANNPTR (0x0007) = 0x2001
PHY 1: ANLNPTR (0x0008) = 0x0000
PHY 1: CR1 (0x0009) = 0x0000
PHY 1: CR2 (0x000A) = 0x0100
PHY 1: CR3 (0x000B) = 0x1000
PHY 1: REGCR (0x000D) = 0x401f
PHY 1: ADDAR (0x000E) = 0x0000
PHY 1: FLDS (0x000F) = 0x0000
PHY 1: PHYSTS (0x0010) = 0x000c
PHY 1: PHYSCR (0x0011) = 0x0108
PHY 1: MISR1 (0x0012) = 0x0000
PHY 1: MISR2 (0x0013) = 0x0800
PHY 1: FCSCR (0x0014) = 0x0000
PHY 1: RECR (0x0015) = 0x0000
PHY 1: BISCR (0x0016) = 0x0100
PHY 1: RCSR (0x0017) = 0x0241
PHY 1: LEDCR1 (0x0018) = 0x0400
PHY 1: PHYCR (0x0019) = 0x0021
PHY 1: 10BTSCR (0x001A) = 0x0000
PHY 1: BICSR1 (0x001B) = 0x007d
PHY 1: BICSR2 (0x001C) = 0x05ee
PHY 1: CDCR (0x001E) = 0x0102
PHY 1: PHYRCR (0x001F) = 0x0000
PHY 1: MLEDCR (0x0025) = 0x0000
PHY 1: COMPT (0x0027) = 0x2001
PHY 1: COMPT (0x003E) = 0x0102
PHY 1: PTPCFG (0x003F) = 0x0000
PHY 1: (0x0040) = 0x6100
PHY 1: TXCPSR (0x0042) = 0x2000
PHY 1: SOR1 (0x467U) = 0x4ec3
PHY 1: SOR2 (0x468U) = 0x0000