Hello Team,
Need your help to provide TI recommend
QSPI interface We use two components on the motherboard.
 These two TI components are SN74CBTLV3257PWR and TMUX154ERSWR.
 Re-evaluating the RISER board requires adding a re-driver or re-timer design mechanism.
Require:
1.SPI Freq: under 66MHz.
2.eSPI voltage is 1.8V;
QSPI voltage is 3.3V.
3.direction needs support bidirectional.
4.QSPI:As briefly mentioned above,
it is recommended whether Riser has a design that can
support similar functions such as re-driver or re-timer.
5.eSPI:There is no special intermediate component processing on the motherboard. It is recommended on RISER whether there are similar recommended design components.
Thanks