Other Parts Discussed in Thread: ALP
Dear team,
Greetings!!!
We are designed our own custom serializer and de-serializer board. As well, We have the DS90UB926 EVK board.
With help of EVK I2C communication we can able to generate display pattern on de-serializer via serializer I2C configuration. So, We ensured both boards and cables are working fine.
We are facing issue, while external(Controller RGB, PCK, DE signal interface with serializer) custom display data generation on de-serializer side using serializer board configuration.
Until pattern generating CDR lock is properly locked. If external PCLK supplied from controller to serializer, then CDR lock link is broken. If external PCLK signal stopped or removed, then CDR lock detected.
Kindly let us clarify below queries ASAP,
- In ALP application, While generating patterns – we need to configure the display timing parameter. In this same way, how can we configure the display timing parameters while generating custom display information(i.e Controller data to display)? Shall we use Pattern generator register also for custom display information or any another way to do?
- If display need 33Mhz PCLK on De-serializer side, then serializer PCLK input also should be in 33MHz range. Is this statement correct? If any wrong in my understanding, kindly let us know formula for serializer PCLK input calculation based on De-serializer output.
- If any example scripting available for this issue, Kindly share to us.
Kindly do needful ASAP.