Part Number: TUSB8042A
Other Parts Discussed in Thread: TUSB8044A, TUSB8040
Hi.
I need EEPROM configuration utility for TUSB8042A USB hub in windows os.
Where Can get this tool?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Would you please accept my friendship request so I can send you the tool in a private e2e message?
Thanks
David
How Can I reconfigure EEPROM after register address 0x0 rom signature value to 0x55?. after writing this value, Cannot access to EEPROM programming utility.
Hi,
Can you force the hub into the programming mode?
Forcing a USB hub into Programming Mode Step
1: Select the USB 2.0 portion of the TUSB8044A hub – it will be the Generic USB hub listed next to the Generic SuperSpeed USB Hub if you set Device Manager to view “Devices By Connection” mode. You can also right click and check the Hardware Ids under Properties, it should be VID_0451&PID_8442. I may have a slightly different version of the silicon, so the PID may be a little different.
Step 2: Once you have the correct Generic USB hub, right click and select “Update Driver Software”, then “Browse my computer for driver software”, then “Let me pick from a list of device drivers on my computer”, and then “Have disk”.
Step 3: When the Install from Disk window pops up, navigate to the TUSB80xx EEPROM Programmer directory (should be under c: Program Files (x86)> Texas Instruments Inc) and select the “TUSB8040.inf” file and open it. Ignore all the warnings and allow the driver to load
Step 4: Open the programming tool.
Step 5: You will need to reload the original Generic USB Hub driver after reprogramming the EEPROM
Thanks
David