Part Number: DS250DF230
Hi,
Q1. When DS250DF230 is configured in 4.9152Gbps data rate using manual mode, and apply 9.8304Gbps signal, the device lock to this input. Is this expected behavior?
Q2. If so, is there any workaround to resolve this problem?
Q3. When DS250DF230 is configured in 4.9152Gbps and lock to 4.9152Gbps data, then the input is seamlessly switched from 4.9152Gbps to 9.8304Gbps, does the device keeps lock state?
(According to my experience, DS250DF230 gets lock to 9.8304Gbps while it is configured 4.9152Gbps rate)
Q4. Assume that 4.9152Gbps and 9.8304Gbps are sent alternately. If you lock at 4.9152Gbps and then change the setting to 9.8304Gbps (for example, in a short time after 100 ms), will you lock at 9.8304Gbps?
Best Regards,
Nishie