Part Number: DS25BR101
Hello team,
What would be the output state, if I input Vcc or GND to both IN+ and IN- pin at the same time?
Best Regards,
Kei Kuwahara
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS25BR101
Hello team,
What would be the output state, if I input Vcc or GND to both IN+ and IN- pin at the same time?
Best Regards,
Kei Kuwahara
Kuwahara-san
Please see the spec below

So for both cases, differential input voltage will be low and output will be low as well.
Thanks
David
Hi David-san,
Thank you for your answer.
However, I am bit confused.
From the table you attached, I think it will be both HIGH when, both input was VCC.
And when both input was GND (0V), it might not determine HIGH or LOW because VTH and VTL are both 0V (TYP).
Is my understanding correct?
Best Regards,
Kei Kuwahara
Kuwahara-san
This is a typo on my part. You are correct that differential output voltage will then be undefined. If you want the output voltage to be in certain state, then you would need to implement external failsafe biasing. Please see this app note, https://www.ti.com/lit/an/snla051c/snla051c.pdf
Thanks
David