Part Number: PCA9543A
Other Parts Discussed in Thread: TS5A23157
Hi,
We have 2 Master 1 slave application as below.
Does PCA9543 can support this application?
Or there have other suitable device?

Thanks!
Jeff
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The two Sx0/Sx1 channels are disabled by default, so the configuration commands must come from the SDA/SCL pins.
If both masters are multi-master capable (i.e., support arbitration and bus-busy detection), then you do not need any mux. Otherwise, use a general-purpose mux like the TS5A23157, which must be controlled with a separate GPIO signal.
Hello Jeff
in addition to what Clemens suggested here is a FAQ that talks about GPIO controlled i2c switches
Is using a mux that is gpio controlled an option?
Regards,
Kameron