This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83869HM: RGMII to 1000Base-KX design for i.MX8MP

Part Number: DP83869HM
Other Parts Discussed in Thread: TLK10232, DP83869

Hello, 

We are considering the following design approach for i.MX8MP to work for a 1000Base-kx. 

This approach involves two ICs. The first IC (PN: DP83869HM) is tasked with converting RGMII signals to SGMII, while the second IC (PN: TLK10232) is responsible for handling SMGII signals and transitioning them to 1000BASE-KX, as illustrated in the accompanying image.

We know that the first IC (PN: DP83869HM) can be used as a bridge (RGMII-SGMII), but we haven't seen detail hardware design guidelines. Do you think this is viable? if so, can you give us the required information to proceed with this design?

By the way, the reason we chose this design is because the i.MX8MP doesn't support either SGMII or SERDES (1000Base-kx).

Thanks,