Part Number: TUSB9261
After having developed a flash programmer which runs on a microcontroller to initialize the SPI flash of its linked TUSB9261, I am trying now to do the same in UFI mode. That is firmware running and with no means to force the HID mode (I do not want to have any jumper as J13 on the demo board in order to simplify the update process).
The user guide of the TI flashburner running on windows mentiones in §3.2 that there are some SCSI commands that can do the same job as in HID mode. I tried these commands with firmware versions 0.99 and 1.06 and it does not work. I am sure it is possible as the flashburner running on windows does it.
In my undestanding UFI and SCSI modes are compatible, am I wrong ? Have you any idea or at least an example of TUSB update in SCSI mode ?
Regards
Meziane