Part Number: DS110DF111
Hello,
I would like to have my VCO free-running to generate a PRBS pattern. If the input voltage and temperature are held constant, can I expect the VCO to output a stable frequency (even if it is not the desired 10.3Gbps)? Or will it drift with even very minor ripple in the supply voltage or temperature?
Thank you!
Best regards,
Zach Kimble