Part Number: TVS3300
Other Parts Discussed in Thread: TSM36A
Hello,
I would like to protect a power line from overvoltage events. Maximum expected voltage on the line is 33.6 V. Firstly I'm thinking about using SMAJ33A diode, which has Vwrm of 33 V, minimum breakdown voltage (voltage where current equals 1 mA) of 36.7 V and maximum of 40.6 V. Maximum clamping voltage for this diode is a little bit higher than 53 V. Although expected maximum voltage on the line is 0.6 V higher than Vrwm voltage of diode, I think that everything would still work great, since there is still a sifficient gap between maximum expected voltage and minimum breakdown voltage. SMAJ36A diode would be a next diode from the list, but it has also higher clamping voltage - I'm using DC/DC converter with absolute maximum input voltage of 50 V and I'm worry that 36 V would not sufficiently protect this converter, because clamping voltage is higher than 50 V.
However, because of limited space on the board, I'm now thinking about using TVS3300 TVS diode for protection, but I'm worry about this idea, because this diode has much more "shaper" characteristic.
What do you think?
Many thanks, Kind regards, Dejan.