Part Number: SN65LVDS31
Hi,
I'm looking at part numbers SN65LVDS31PW and SN65LVDS32PW and I don't seem to see the maximum junction temperature. I see a max operating temp of 85C, but I'm not sure if this is referencing the max junction temperature or the maximum case temperature. Oftentimes, maximum operating temperatures don't correspond to maximum junction temperatures, as junctions can go to higher levels. Seeking clarification if the operating temperature for these two is indeed the max junction temp. Thanks!