Part Number: AM26LS32A
Other Parts Discussed in Thread: AM26C32
Hi,
Our customer is confirming the 4M change point about AM26LS32A.
Q1
Due to the change from datasheet Rev.F to G,
From the graph of 6.8 Typical Characteristics (below, left: Rev.F, right: G),
Ioh: 0mA ~ -25mA
In the range of , the Voh level has increased by nearly 1.5V after the change.
Does this mean that the elements up to Rev.F also had drive ability at the level of the graph on the right? Or is it due to design changes?
Q2
The process has been changed to LBC9 (CMOS), but is the previous process also CMOS?
I think the LS family was initially bipolar.
Best regards,
Hiroshi