Part Number: DS320PR1601
Hi,
In the datasheet of DS320PR1601, on page 17 under section 6.5 DC Electrical Characteristics, I (TX-SHORT) is given as 70 mA.
Is this the maximum current drawn by the redriver?
Thanks and Regards,
Shekha Shoukath
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS320PR1601
Hi,
In the datasheet of DS320PR1601, on page 17 under section 6.5 DC Electrical Characteristics, I (TX-SHORT) is given as 70 mA.
Is this the maximum current drawn by the redriver?
Thanks and Regards,
Shekha Shoukath
Hi Sheka,
Technically I believe this could be interpreted as the maximum current drawn by each TX line, but in practice I don't think they should be shorted to ground without a termination resistor in between. So in operation I would expect the TX currents to be significantly lower than 70 mA. As a quick and rough reference, the typical power consumption with moderate to high EQ is given as 5.8 Watts. At 3.3 V power supply, this would be equivalent to about 1.76 A drawn from the power supply. If we divide this by 32 channels, the result is about 55 mA, and this does not account for the overhead from other device subsystems so the true per-channel current draw should be less than that. However I don't think we have this information available.
Best,
Evan Su
Hi,
Thanks for the reply.
Could you please tell the maximum current drawn in a DS320PR1601RSCEVM module.
Regards,
Shekha Shoukath
Hi Sheka,
I don't think this has been measured explicitly. The maximum power consumption with EQ 5-19 and all channels active is given as 7 W, which at 3.3 V supply voltage would be equivalent to 2.12 A, this may be considered an upper bound on the current draw for the entire device.
Best,
Evan Su