Part Number: TCAN1044AV-Q1
Other Parts Discussed in Thread: TCAN1145-Q1
Hi,
As per the transceiver datasheet wakeup monitor needs VCC < UVVCC along with STB driven to HIGH. Typical UVVCC is 4V.

Below is the waveform captured Ch 1 – CANH signal, Ch2 – CAN_RX on CAN transceiver when STB pin driven to HIGH.
Looks to be as VCC < UVVCC condition is not met, the RXD pin is reflecting (mirrors) the same signal of CANH/L.

Also, datasheet mentions “In standby mode, only the VIO supply is required therefore the VCC may be switched off for additional system level current savings.”
Is it necessary to have either VCC to be turned OFF or VCC < UVVCC on the CAN transceiver to have the CAN wakeup monitor feature?
Thanks,
Kantha