Other Parts Discussed in Thread: TRSF3232, TRS3227E,
I am using the parts mentioned above to provide LVDS signaling over a long length of Cat5E cable (4 signals total). The LVDS segment seems to work well. Two of the signals originate from a laptop using a standard serial port - RS232. I believe to accurately get the RS232 signals to a format for using the LVDS circuit, I need a component like your TRSF3232 part. I've included a schematic showing the connections of the 3 parts mentioned. Connector J1 is the db9 header that connects to my laptop serial port. Then the RS232 interface chip, then you can see the LV047 and LT012 chips. Connector J2 over on the right is an RJ45 connector that has the LVDS outputs.
Before I make the test PCB to try this, I wanted to confirm (or at least get your opinion) that the circuit I have shown is what is expected for RS232/LVDS interfacing.
Sincerely,
Peter