For ds90ub962-q1, if the input is rgb888, can it be converted to yuv422?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Ray,
for these SER-DES devices, everything comes in will be bypassed to the output. We do not have data type conversion.
hi Hamzeh
I see that 940 can perform these conversions. May I ask if 962 is possible?
Hi Ray,
the 940 is from different family, this is an IVI device. But the 933/953 and 962 are from ADAS family which does not support data type conversion.