Part Number: DS110DF111
Other Parts Discussed in Thread: DS100DF410, , DS110DF410, DS125DF410, DS125DF111
Hello
I can use SMBus read register.
I refer to "DS110DF111, DS125DF111, DS100DF410, DS110DF410,and DS125DF410 Programming Guide"
2.4.1 Front-Port Ingress (Module-to-Host)
2.4.2 Front-Port Egress (Host-to-Module)
2.4.3 Backplane and Cable
Table 20. Set Data Rate(DS125DF410 as example)
and use 10G,SFP device connection
but I tried several ways, Reg_0x54[7] always 0
can you help me, how to setting register,
the following is channel register status.
Hex 0 1 2 3 4 5 6 7 8 9 A B C D E F
00 | 00 00 00 00 00 00 00 00 00 00 10 0F 08 00 93 69
10 | 3A 20 A0 90 00 10 7A 25 40 23 00 03 24 00 E1 55
20 | 00 00 00 40 40 00 00 00 00 00 30 00 72 80 00 06
30 | 00 40 11 88 3F 1F 33 00 00 00 A5 00 00 00 80 00
40 | 00 40 80 50 C0 90 54 A0 B0 95 69 D5 99 A5 E6 F9
50 | 00 00 A5 00 00 00 00 00 B0 95 ED D5 99 A5 E6 F9
60 | 00 00 00 00 00 00 00 00 00 0A 44 40 00 00 00 00
70 | 03 20 00 00 00 00
Control and Shared Register
Hex 0 1 2 3 4 5 6 7 8 9 A B C D E F
00 | 00 60 -- -- 01 00 00 04 -- -- -- -- -- -- -- 00