Dear Driver developer
If the RS485 driver on the A side is shorted between VCC and B (or shorted between GND and A) and the B side is operating normally, is there a possibility that the A side driver will be damaged if communication starts between the A side and the B side?
This state is a combination that is not found in FUNCTION TABLE (OUTPUT = A, B both "H" or both "L").
I recently manufactured a device that is MSL Level-1 (Unlimited) and is 7 years old.
Is there a possibility of damage due to not baking?SN65LVD3082ED_Circuit.pdf