This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power over Data Line - PD Design Application Note SNVAA25A

Hello,

I have a question regarding Figure 3-8 (PSE start-up Behaviour) in the Application Note SNVAA25A (IEEE 802.3cg 10BASE-T1L Power over Data Lines Powered Device Design).
According to the figure tje PSE output current rises above the prebias valid criteria (= current consumption between 1.25mA and 1.85mA) after the prebias gets enabled.
But after approx. 3ms the current consumption decreases and meets the prebias valid criteria (see yellow rectangle). How is this step implemented?