1.DS90UB953 can support DVP mode, which means that the sensor inputs MIPI signals to 953, and enables the 953 chip to output DVP for back-end unstring by configuring its relevant registers. Do you need special design on the hardware circuit? Please refer to the reference design on your official website. One copy is MIPI, but the GPIO is also connected with VSYNC?
2. We are now MIPI 2LANE, and the default reference for DS90UB953 is 4LANE. Is there any special requirement for signal channel hardware connection for our application using 2lane?
3. The manual only describes the current parameters of 4lane, does this have the current parameters of 2lane?
4. The manual only says that the operating frequency range is 25~104MHz, and the frequency range of independent crystal oscillator is recommended to be 24.2~25.5MHz. Is there any specific PPM requirement for this?
5. Have the latest design application guide and PCB design guide;