Part Number: TUSB320
Hi, TI support team
My customer asked product that is possible for current control thru CC1, CC2.
TI product is TUSB320.
Operating senario that he want to design is below.
- USB A(Adaptor) to USB type-C(Device) : Charging under 2.0A
- USB type-C(Adaptor) to USB type-C(Device) : Charging 3.0A
When using CC control, is it possible to control to change only the current?
Do I need to change the voltage through CC control?
Charger is a product that has an input range of 13V.
From what I've searched, it seems that the TUSB320 product is possible, but if there is a suitable product, please recommend it.
Thanks.
Regards,
MJ