This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964-Q1: DS90UB964-Q1 Power supply rails description required

Part Number: DS90UB964-Q1


Dear Team,

Below is the power supply rail names of  DS90UB964-Q1.

Could you please give description of each rail.

Power Rails Description
VDDIO VDDIO is the voltage that IO can accept
VDD_CSI0
VDD_CSI1
VDDL1
VDDL2
VDD_FPD1
VDD_FPD2
VDD18_P2
VDD18_P3
VDD18_P1
VDD18_P0
VDD18A
VDD18_FPD0
VDD18_FPD1
VDD18_FPD2
VDD18_FPD3

Regards

HARI

  • Hello Hari,

    Why do you need the descriptions?

    Due to upcoming holidays, please allow until the end of next week so I can collect what is possible from these details.

  • Hi Hamzeh,

    Please take your time.

    I am making a hardware design document for my board.

    Regards

    HARI

  • Hello Hari,

    See below:

    VDD_CSI0 1.1V Supply for CSI-2 Port 0
    VDD_CSI1 1.1V Supply for CSI-2 Port 1
    VDDL1 1.1V Digital Supply
    VDDL2 1.1V Digital Supply
    VDD_FPD1 1.1V Supply for FPD Port 0/1
    VDD_FPD2 1.1V Supply for FPD Port 2/3
    VDD18_P2 1.8V Digital Supply
    VDD18_P3 1.8V Digital Supply
    VDD18_P1 1.8V Digital Supply
    VDD18_P0 1.8V Digital Supply
    VDD18A 1.8V Analog Supply
    VDD18_FPD0 1.8V Supply for FPD Port 0
    VDD18_FPD1 1.8V Supply for FPD Port 1
    VDD18_FPD2 1.8V Supply for FPD Port 2
    VDD18_FPD3 1.8V Supply for FPD Port 3

    Please note though that removal of any supply connection to the IC is invalid, even if certain ports/functions are unused. It is always required to supply all power rails to the device 

    Best Regards,

    Casey 

  • Hi Casey ,

    Thank you very much.

    Regards

    HARI