Part Number: TCAN1463-Q1
Hello team,
A customer asks about the resistor power size installed for split termination on the sub node of CAN bus.
1/16W is acceptable for 1.3kohm? Otherwise, what is the optimal value?

Thanks and regards,
Sam Lee
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCAN1463-Q1
Hello team,
A customer asks about the resistor power size installed for split termination on the sub node of CAN bus.
1/16W is acceptable for 1.3kohm? Otherwise, what is the optimal value?

Thanks and regards,
Sam Lee
Sam,
This can be determined using the specific fault conditions that the designer expects. Generally in normal operation, no more than 5 V will be present across the resistors, so you would need them to be able to withstand a 5 V potential difference at DC without damage. If their node uses 2.6 kΩ termination, this would correspond to (5 V)^2/(2.6 kΩ) ≈ 9.62 mW which should be fine for most resistors at 1/4 W. However, if your OEM specifically requires other conditions (such as a specific worst-case DC Vdiff), then you'd need to design for that worst-case DC condition.
Best,
Danny