Hi Team,
We are using LIN trx like TLIN1021A-Q1 in numbers of applications.
When the power supply is normal, MCU want to configure EN pin to enter sleep mode. While if there is signals on LIN bus, there would be some problems:
Right now the MCU already let TLIN1021 entered sleep, the signal on LIN bus cannot be received by MCU. While the voltage on LIN bus will trigger TLIN1021 INH pin pulled high. We would like to learn if there is any method that can let the MCU receive the LIN bus data when sleep mode(not through INH pin). Or can we make MCU let TLIN1021 enter sleep mode and then isolate the LIN bus to reject all of the signal/data from LIN bus?
Thanks
Best,
Frank