Part Number: DP83848Q-Q1
Hi ,
DP83848Q-Q1
100BASE-TX PHY can we use the part number for vehicle interface communication replacing CAN.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83848Q-Q1
Hi ,
DP83848Q-Q1
100BASE-TX PHY can we use the part number for vehicle interface communication replacing CAN.
Hi Ajay,
Could you provide me with more information about what your design requirements are? A block diagram would be greatly appreciated.
Regards,
Alvaro
Hi ,
I need a part which can replace CAN interface for vehicle interfacing. will this part be okay for vehicle interfacing?
Hi Ajay,
Yes, the DP83848 can be used to connect two interfaces via a standard ethernet cable.
MAC <-> DP83848 PHY <-> RJ45 Ethernet Cable <-> Receiving Board/Interface
The standard RJ45 ethernet cable uses 4 twisted pairs for communication.
There is another type of ethernet cable used in automotive applications called MATEnet. This uses a single pair cable and WILL NOT work with the DP83848.
Please see our PHY Selection Tool to filter our other Automotive PHYs. The DP83848Q-Q1 is the only automotive PHY that uses the standard RJ45 connector.
Regards,
Alvaro