Part Number: THVD1429
Other Parts Discussed in Thread: THVD1400, THVD1420, THVD2410
Hi,
We are using THVD1429DR RS485 IC with CC3220MODSF12MOBR.
We are reading 30 parameters (1 Packet) from slave Device. Frequency: 1 parameter per sec. Baud Rate 9600 bps.
We are noticing some issue while reading the data from the slave devices. Mean, some Parameters are some times not receiving, but most of the time we missing parameters, we cant guess which parameter to be missed. In missed parameter we are printing the reasons. reason will be Slave not responding, Extra size,etc.
But same slave device modbus connected with PC using USB to Modbus Converter all the 30 parameters received without fail, all the time.
I have replaced 220 Ohm ferrite bead with 0 Ohm Resistor and also we tried with populating 523 Ohm Resistor on R12, R13. But printing same issue.
Please find the schematic FYI. Kindly advice to resolve this issue.