Part Number: DP83849IFVS-EVK
Other Parts Discussed in Thread: DP83869
Hi experts!
I was having an issue in the connector.. the communication is happening when i put cable connector like as shown in the below image and if i fully insert it won't work..

the connector which is used in the DP83849IFVS-EVK is AFBR-5803Z
first i thought it's a connector issue but it's actually the cable issue..
i was thinking SC cable will be standard cable and it can be used anywhere with the sc type connector.. but it was not worked with my existing cable..
It is working when i connect another locally purchased DX 3.0mm which doesn't have datasheet and SC-1 written on it..
It is not working when i connect with SC-P, SCC-1 name written on connectors..
i would like to know in-detail about it, can you please share any resources where i can find all the types of SC connectors..
i'm still thinking on is that the connector issue or the cable issue, because i have a link partner "D-LINK" it is working with all types of sc connectors which i mentioned above..
Thanks & regards,
Tex