Part Number: TCAN4550
Hello,
Our system is using 5V as main voltage. We don't have 12 or 24V Vbat. Is there a way to use TCAN4550 with 5V supply without Vbat?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Serhan,
Unfortunately no, there is no way to use 5V directly with the TCAN4550-Q1 because there is an internal 5V LDO that requires at least 5.5V on VSUP. There is not a way to bypass this internal LDO and directly supply an external 5V supply. You would likely need to use a Boost Converter to generate a VSUP supply voltage greater than 5.5V to prevent the TCAN4550 from seeing an under-voltage condition and entering a protected operating mode.
Regards,
Jonathan