Part Number: DP83826I
Set to BASIC mode. I want to use Strap2 with Auto Negotiation Enable.
Are the LED lighting circuits for LED0 (Strap2) and LED1 (Strap1) correct?
Please check the circuit diagram.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83826I
Set to BASIC mode. I want to use Strap2 with Auto Negotiation Enable.
Are the LED lighting circuits for LED0 (Strap2) and LED1 (Strap1) correct?
Please check the circuit diagram.

Hi Satoshi,
Both LED0 (Strap 2) and LED1 (Strap 1) are default '1'; Auto-negotiation Enable and 100M speed respectively. Is the 3.3V supply through R142 & R143 meant to go to the pins through the Green and Yellow diode? Even so, it will keep both Straps in a high state, which is what you desire.
Regards,
Alvaro
>Is the 3.3V supply through R142 & R143 meant to go to the pins through the Green and Yellow diode?
Yes. That's how it is.