Part Number: HD3SS3412
Other Parts Discussed in Thread: TS3DV642
Hi team
Does HD3SS3412 support MIPI HS and LP?
LP is single end signal 1.2V
Thank you very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mr. Liu,
The HD3SS3412 is designed for differential signals only. I recommend using TS3DV642 for single ended signals.
The TS3DV642 is a device that can support single ended signals. It can pass any signal as long as the signal swing voltage is within (0-5.5V), the bandwidth is (<7.5 GHz), and the current is (<128mA). Please double check and make sure signals are within the recommended operating conditions as stated in the datasheet.
If you use this device, pass the single ended signal through the + line and leave the corresponding - line floating.
Best,
Shane