Part Number: LMH1297
Dear Nasser,
Long time no see, how are you ? I hope you are very well?
I've recently been using LMH1297 as an interface chip for optical transmission, and I've had a problem that hasn't been solved:
the quality of the eye diagram is poor (relative to PIN8) when the input port of the LMH1297 is configured as the output.
I suspect it's the influence and interference caused by the internal EQ circuit to the CD circuit, but the EQ function has been turned off, so I don't know if there is any other workaround
Thanks Nasser,
KindRegards!
WangChen.