Part Number: TCAN1463-Q1
Other Parts Discussed in Thread: AWR1843AOP, , TCAN1146-Q1
Hello, I am a beginner using TCAN1463-Q1 and awr1843aop.
In my application, when the radar sensor receives power, it sets the nSTB and EN pins to high.
The issue is that when any CAN message is received from the CAN bus, the radar sensor transitions to normal mode.
Therefore, I am checking the message ID upon reception and trying to switch back to sleep mode.
However, when continuously sending messages through PCAN with intervals less than 93ms, the radar sensor does not transition to sleep mode and remains in normal mode.
Simultaneously, there are errors in both the transmission and reception of messages.
Based on my assumption, The BUCK Converter is controlled by the INH pin, and since the INH pin is continuously toggling between on and off states,
the 5V voltage supplied to VCC appears to be fluctuating but not dropping below 4.5V(minimum operating conditions).
I would appreciate it if you could confirm whether this speculation is correct, and kindly provide information on any other possible causes.
Thank you very much.