Part Number: DP83TC812R-Q1
Hi, TI Expert.
As title description, we already know DP83TC812R support "RGMII tx/rx internal" delay base on different "hardware bootstrap pin" setting.

Question 1 : Could we also change "RGMII tx/rx internal" by register setting without bootstrap pin? (y/n)
If the answer is "yes", and then "How to do it"?
Question 2 : Does register A2D_REG_48 (Address = 0x430h) do an additional setting for "RGMII tx/rx internal"? (y/n)
I must make sure "RGMII tx/rx internal" work, and then "A2D_REG_48" works, Is it right?(y/n)
CLK shift 90 degree, the default value should be 111b.

Question 3: Need sample code to access A2D_REG_48.
Already download code here, and try to modify some bug base on these two link.
We found these driver do not support A2D_REG_48 setting, Could you give us some example?
Many Thanks
Gibbs