Part Number: SN65DPHY440SS
Dear Sir,
Just like the title, can SN65DPHY440SS work at 2 lanes mode?
Best regards.
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: SN65DPHY440SS
Dear Sir,
Just like the title, can SN65DPHY440SS work at 2 lanes mode?
Best regards.
David
David
Is this a DSI or a CSI application? Both DSI and CSI can support 2 lanes mode. But for DSI, one of the four lanes is used for back channel communications between GPU and DSI panel. DPHY440’s lane 0 is the only lane that supports the back channel. For this reason, DPHY440 lane 0 must always be connected to lane 0 of GPU and panel.
Thanks
David
HI,David,
CSI,not DSI!
It seems no pin or registers to configure,how to do that?
Best regards
David
David
Please see below for the CSI 2 lane example. There is no pin or register to configure DPHY440 for the 2 lane mode. You just need to tie unused input to ground and unused output floating.

Thanks
David