Part Number: DP83867IR
Hi,
I am using a 3rd party board that has a DP83867IRPAP PHY. We occasionally see issues with our product in the form of Ethernet links not coming up or huge power consumption increases (according to an input current monitor) with the PHY increasing ~35 degrees Celcius on on the package (according to a thermocouple).
We have identified 2 issues with the schematic and are wondering the impact of them.
The first and most obvious mistake is that the magnetics integrated in the jack used are for current-mode drivers, and contain a ferrite bead to 1.8v. Of the 2 times I've been able to get logs off of our system after, I saw in both cases the PHY downshifted to 100Mb and the Linux driver complained to check cabling. Not only is there this ferrite bead, but also the center taps of the first set of transformers are all shorted together (and then go to the bead). We are wondering about impact of this mistake. I've seen This forum post and the recommendation not to tie them together. However, I'm still wondering about what we can see.
The other problem is that this board uses the old recommendation of 1 nF capacitors. Can more information be shared on why TI increased the recommended values?
Thank you