Part Number: ESD321
As shown in the figure below, there is a significant difference in the ESD junction capacitance for the USB interface in TI's ESD protection devices. With different IEC 61000-4-2 electrostatic testing conditions, the recommended ESD diode junction capacitance also varies;
Please help confirm if the static electricity testing requirements are different, and the corresponding junction capacitance is also different. Thank you;