Part Number: TRS3122E
Hi Team,
Is the TRS3122E correct socket to achieve UART to RS232?
Do we have one channel socket can be promoted?
Regards,
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TRS3122E
Hi Team,
Is the TRS3122E correct socket to achieve UART to RS232?
Do we have one channel socket can be promoted?
Regards,
Roy
The search function shows that there are indeed 1+1 transceivers:
ti.com/interface/rs-232/products.html#286=1;1
(The SNxxx devices are old; the MAXxxx and TRSxxx devices are identical.)
What supply voltage, data rate, and ESD protection do you need?
Hi Roy,
The most common application using 1 channel RS-232 is UART - so the TRS3122E can be used to to convert between UART and RS-232 as long as your application needs fit into the performance range of the TRS3122E
A couple notes to help with determining if this is the right part:
1. The TRS3122E can be supplied by a voltage supply of 1.65V to 5.5V; ac integrated charge pump (needs external capacitors) will generate the output swing voltages for RS-232. Generally you would pick a supply that matches the controller connected to the transceiver - this is a wide VCC RS-232 device though so it covers most controllers in the 1.65V to 5.5V range.
2. A 1Mbps data rate can be achieved with a capacitive loading of 500pF and 500kbps can be achieved with a capacitive loading of 1000pF - above that and the data rate could suffer. In general most of the capacitive loading is from the cabling - it is generally assumed that RS-232 cabling is usually about 167pF/m (but check your specific cabling datasheet for more information). So essentially 1000pF would be about ~6m bus using common RS-232 cabling. So depending on data rate and max bus length (+ cable properties) needed in the application will help determine if this is the best part.
So if you could confirm the following for me I can also verify if this is our best part for your specific application:
1. What is the voltage supply needed?
2. What is the bus length for the RS-232 portion
3. If using cabling - do you have a part number so I can look up the datasheet?
4. What data rate will the UART be running at?
Generally speaking many UART applications are handled just fine by RS-232 - but I would like to verify the above information to see if this is the best part for this specific application.
Best,
Parker Dodson