This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822IF: LED_0 and COL pin Configuration

Part Number: DP83822IF


Hello,

I need to set LED_0 of DP83822IF to MII_LINK

and i need to set COL to operate as LINK_OK

When I looked at the datasheet, I understand that LED0 and COL pins are set in the MLEDCR register.

However, if I look at page 52 of the data sheet, it says “MLED can be routed to only noe of these two pins at a time.”

I understood that MLED settings were only possible with either LED0 or COL. Is that correct?

thank you