Other Parts Discussed in Thread: UNIFLASH, CC3200, , CC3100
Hi there,
I've only seen this issue on E2E a couple times, with no actual resolution.
In attempting to connect to the CC3200 using UniFlash (3.4.1), I am getting the following:
[17:25:14] Begin ServicePackProgramming operation.[17:25:15] INFO: > Executing Operation: Connect[17:25:15] FATAL: --- Can't connect to device !! ---[17:25:18] FATAL: Error connecting to the device. Please check your COM port settings. Error code: 1[17:25:18] INFO: > Executing Operation: Disconnect[17:25:18] Operation ServicePackProgramming returned.[17:25:51] Begin ServicePackProgramming operation.[17:25:52] INFO: > Executing Operation: Connect[17:25:54] INFO: setting break signal[17:25:55] INFO: detecting FTDI for device reset[17:26:11] ERROR: ---reading ACK signal failed---...[17:52:46] WARNING: ---seting break signal to false failed---[17:52:48] INFO: setting break signal[17:52:49] INFO: detecting FTDI for device reset[17:53:05] ERROR: ---reading ACK signal failed---[17:53:05] WARNING: ---seting break signal to false failed---[17:53:05] FATAL: --- Can't connect to device !! ---[18:06:06] FATAL: Error connecting to the device. Please check your COM port settings. Error code: -3[18:06:06] INFO: > Executing Operation: Disconnect[18:06:06] Operation ServicePackProgramming returned.
I've tried resetting the launchpad, with and without SOP2 Jumper, with and without J8-J11.
I have successfully connected to the device on MacOS in the past as well, but the failed ACK is occurring there now too as the CCS debugger is no longer connecting. I've also tried using cc3200tool but ACK failed there too.
Can anyone describe what's happening? I suspect something is wrong with the FTDI device on the Launchpad, but can't find enough information in the documentation to figure it out.
Thank you!