Other Parts Discussed in Thread: AM3352
I believe your company is conducting a mactest (margin test) for ethernet,
is it possible for us to receive the results?
Best regards.
Toda.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have not heard of such a test,
Sincerely,
Gerome
Thank you for your reply.
Never heard of mactest?
Does that mean there are no test results?
If you don't have them, do you know the steps on how to do this test?
By the way, mactest is like as the following.

Hello,
What you are describing is throughput test. While you will need to consult with the MAC vendor for how to enable traffic, for external loopback you will need to connect external cable to RJ-45 with RX pins shorted to TX pins. For PHY loopback, MII loopback (Reg 0x0[14]) is only required.
Sincerely,
Gerome
Hello,
Thank you for your reply.
Do you have the throughput test results?
If you have them, could you send me?
Best regards.
Hello,
We do not have documented results for tests like these. Have you conducted these tests on your board? If so, are you having issues?
Sincerely,
Gerome
Hello,
No, we have never conducted such a test.
Could you give me some advice on how to conduct throughput test?
Best regards.
Hello,
For this test, you will need to consult with the MAC vendor to enable traffic. From a PHY standpoint, the only procedure needed is for PHY loopback, where Reg 0x0[14] = '1' for MII loopback. Otherwise, PHY configuration is default.
Sincerely,
Gerome
Hello.
Do you mean that MAC vendor is the microcomputer manufacturer that connects to PHY?
We use AM3352. This is also your product.
Best regards.
Hello,
I can reassign this thread to the appropriate contact to take up further.
Sincerely,
Gerome
Hello Takafumi Toda,
Can you help me understand if you are checking if MAC loop back is supported or you are looking for some specific performance?
Is there a use case for the query that you could share for me to check internally.
Regards,
Sreenivasa
Hello.
I want to check if MAC loop back is supported for AM3352.
If it is supported, please let me know how to configure it.
Best regards.
Hello Takafumi Toda,
Thank you.
I will have to check internally and assign to an expert.
Any thoughts if you are interested in ICSS or CPSW interface?
Regards,
Sreenivasa
Hello,
Sorry for late reply.
Could you check with the CPSW interface?
Is this supported 1000BASE-T?
Best regards.
Hello Takafumi Toda,
Thank you.
I am assigning to the CPSW expert to answer.
Regards,
Sreenivasa
Hi,
I am basing my answer on the diagram above discussing u-boot. In my experience I have not heard of mactest in a u-boot context. Doing a brief search I only one instance of mactest in a competitor specific source tree in u-boot.
From a Linux context TI reviews performance during SDK release testing using standard Linux utilities. Ti does not do MAC testing in the u-boot context.
TI does provide MAC loopback testing SW as part of the MCU+ SDK that has source code that the customer can compile. Here is a link to CPSW section of the user guide describing loopback testing. This code is not part of a u-boot/Linux environment.
Best Regards,
Schuyler