Part Number: DS90UB953A-Q1
Hi team,
We have an question about the S21 in 95x channel requirement file below, for instance, if the forward channel rate is 3Gbps(1.5GHz), how to compare the real test result of customer's board with our requirement? How to ensure the requirement which are not included in the example point below such as 1.5GHz, 1.7GHz, etc.