Part Number: MAX3232
HI sir,
When the RJ45 cable is not connected, the IC can function normally without sending random messages.
But after connecting it(only cable) and turning DUT on (but not connecting to USB-PC), the text "e" will be entered inside the DUT.
Here is Circuit

1.plug RJ45 cable only

Wait for 1 minute (it will not start normally) and then connect RS232 (USB TYPE) to PC
You will find that it keeps sending text "e".
But when we connect RS232 to PC, the text will stop.

2.plug RJ45 cable with RS232(USB type) to PC

normal

thanks!
Vincent