Part Number: DP83822I
Hi Team,
Please tell me the procedure of BIST.
Is the following order correct?
If no, please tell me the correct procedure.
1) Set packet length through [10:0] of the BICSR2(Register address 0x001C)
2) IPG settings through [7:0] of the BICSR1(Register address 0x001B)
3) Enabling BIST error counter mode through [14] of the BISCR(Register address 0x0016)
4) Enabling PRBS Checker through [13] of the BISCR(Register address 0x0016)
5) Enabling Loopback mode through [14] of the BMCR(Register address 0x0000) [14] or [4:0] of the BISCR(Register address 0x0016)
6) Enabling Packet Generation through [12] of the BISCR(Register address 0x0016)
7) Read error byte through [15:8] of the BICSR1(Register address 0x001B)
Best Regards,