Part Number: TDES954
Is it possible to configure the TDES954 for 600Mbps per line and using 4 lanes to have a total of 2400Mbps?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDES954
Is it possible to configure the TDES954 for 600Mbps per line and using 4 lanes to have a total of 2400Mbps?
Hello Cyrill,
The TDES954 supports only the listed rates below. Other rates are not supported:
Based on the REFCLK selection 23-26MHz:
REFCLK*16 = 368-416Mbps/lane
REFCLK*32 = 736-832Mbps/lane
REFCLK*64 = 1472-1664Mbps/lane
You can use the REFCLK*32 or REFCLK*64 gears to support >=2400Mbps total throughput
Best Regards,
Casey